AXIS#.TUNING.INERTIA.STATE

Description

AXIS#.TUNING.INERTIA.STATE indicates which step the Inertia Measurement algorithm is currently in.

Possible Values of AXIS#.TUNING.INERTIA.STATE
Value Description Cause
-2 Error – Bad Data There was an error recording the data for the measurement. Check the wiring and repeat.
-1 Error  Something went wrong in the process. Repeat.
0 Idle  Inertia Measurement has not been run. 
1 Measuring Inertia  Inertia Measurement in progress. 
2 Processing Data is being processed in the background
3 Done  Inertia Measurement process completed successfully. 
4 Done - Clamped Inertia Measurement Completed successfully but was clamped by the AXIS#.TUNING.INERTIA.MISMATCHMAX setting

Versions

Action Version Notes
Implemented 02-13-01-000 

-

General Information

Type Read Only
Units N/A
Range -2 to 4
Default Value 0
Data Type Integer
See Also AXIS#.TUNING.INERTIA.MEASURE
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.TUNING.INERTIA.STATE

5021h

04h

Unsigned8

-

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5045

1

5045 (0x13b5)

AXIS1.TUNING.INERTIA.STATE

Signed16

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.TUNING.INERTIA.STATE

5045

Signed16

Read Only

-